Other Parts Discussed in Thread: OPA2677, , TINA-TI, OPA2675
Tool/software:
Hello,
a while ago I discussed a driver for a small thermoelectric cooler ("TEC" or peltier element). The circuit was based on two inverting current-feedback amplifiers (OPA2677) in a bridged configuration, see the discussion here. So by driving the circuit with a control voltage of say 0 to 3.3V, the TEC could either cool or provide heat.
Putting this circuit into practice, it showed that the power delivered was just not sufficient. The TEC rather acts as a 2 Ohm load and as such only 40 mW (about 280 mV across at 140 mA) could be delivered to the TEC.
I'd like to be able to provide twice as much power to the TEC.
However, the OPA2677 has a max. abs. rating of Vcc = 6,5 V so increasing the supply voltage is not an option.
Sticking to the concept, I replaced the OPA2677 with the THS3121, which is also a high power current feedback amplifier:
The simulation shows that this amplifier is able to provide more than enough power to the TEC:
However, my simulation uses a 6.5 V supply voltage and while the simulation looks good, the datasheet states a minimum supply voltage for single supply operation for this device of 10 V.
Will the THS3121 work with a supply voltage below this minimum (as simulated)?
I could increase VCC to 12 V but this would increase the power dissipation in each THS3121 to about 5.5 V * 0,4 A = 2,4 Watt at the maximum. Please correct me if my calculation is off. This would exceed the max. ratings in the dissipation table:
Note: in the table, I assume the "685 W" is a typo and should read 685 mW.
Any ideas on how to boost the output of the op amp are welcome. Could the output of the op amp be increased by "booster transistors"?
Thanks and have a nice weekend!
Daniel
Please note: I attached the Tina-TI simulation file below.