Part Number: INA226
Tool/software:
I have a system running off a battery. In order to save power, we are disabling the bias supplies.
This means that the INA226 has the following voltages at these pins:
Vs - disabled bias supply (approx 0VDC)
Vbus - battery voltage + (approx 4VDC)

the INA226 works properly, however, when sending the shutdown command to the configuration register (bits-02 = 0) and verifying the command has been written
into the register, the INA226 continues to draw a few hundred ua of current.
is there a problem if voltage exists on Vbus but not on VS (the docs indicate that this is not a problem) ?