This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6525: LMH6525

Part Number: LMH6525
Other Parts Discussed in Thread: LMH13000

Tool/software:

Hi, Advise

I’m building a system to drive four ROHM RLD65NZX1 laser diodes (650 nm, 7 mW output, ~25 mA typical drive current) with closed-loop intensity control via their integrated monitor photodiodes.

My setup includes:

  • ESP32 microcontroller

  • External DAC (e.g., MCP4725 or MAX5217, I²C-controlled from ESP32)

  • Texas Instruments LMH6525 laser diode driver.  Suggest me laser Driver for this setup.