8764.Schematic For Applications Support.pdf
Any help is appreciated on this one. The OPA1642A is specified with 10^13 Ohms common mode and differential mode input impedance, and less than 20pA of input bias current. Why in the world would the non inverting inputs be drawing more than 1.5uA? The resulting differential DC signal at the inputs causes the outputs to rail, eating up all of my dynamic range.
This circuit works perfectly with many other op amps, but they have higher noise floors than the OPA1642.
If the attachment didn't work, here's the link to the schematic: http://dl.dropbox.com/u/20553231/Schematic%20For%20Applications%20Support.pdf
Thanks,
Dan