This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OP07: Abnormal

Part Number: OP07

Tool/software:

During production, an abnormal phenomenon occurred on a batch of motherboards after power-up. The same batch of motherboards used two different printed OP07 chips, and the problematic ones were from the same batch of OP07. The principle behind this is as follows:

‌Figure 1 Schematic Diagram

1.The defective chips were identified as part of the same incoming batch, marked with the silkscreen code ‌"52M"‌ (as shown below).

‌Figure 2  

2.In this circuit, the OP07 chip uses a total of 5 pins, with pins 1, 5, and 8 left floating: Pin 4: Power supply (-15V) Pin 7: Power supply (+15V) Pin 3: Ground These three pins show normal voltage levels. However, pins 2 and 6 exhibit abnormalities. The waveform diagrams for pins 2 and 6 of the OP07 chip with the "52M" marking are shown below:

    

‌Figure 3  ‌Abnormal waveform at Pin 2 of the op-amp

‌Figure 4  ‌Abnormal waveform at Pin 6 of the op-amp

3.After replacing with an OP07 marked "52K," all voltages returned to normal. The silkscreen of the "52K" OP07 is shown below:

‌Figure 5  ‌Silkscreen Comparison

4.The normal waveform between Pin 2 (inverting input) and Pin 6 (output) of the OP07 in the same circuit is as follows:

‌Figure 7 ‌Normal waveform at Pin 2 of the op-amp

‌Figure 8  ‌Normal waveform at Pin 6 of the op-amp

The OP07 chips from the same batch with markings "52M" and "52K" exhibit differences, which caused the abnormal behavior in this circuit.