Part Number: PGA113
Tool/software:
Hi,
In the documentation it is not clear that Vref pin can be connected to GND via a suitable size capacitor to achieve AC signal programmable gain only while keeping a unity DC gain. Assuming that CH1 is used as the active input with an AC signal biased at a DC level AVDD/2, and Vref pin is connected to GND via a capacitor, can we expect to see programmable amplified AC output at the Vout pin which is biased at AVDD/2 (ie programmable gain is applied only to AC part of the CH1 pin signal and unity gain is achieved on input DC signal)?
Thanks.