Part Number: ALM2402-Q1
Tool/software:
This is a follow-up question for Jacob who helped me get this far...
The circuit you provided does work as intended when there's no load. However, it does not provide enough current to get the DC-DC converter running. Although the spec for the G60 supply says that it should start at about 0.7V and run at 175 mA with no load. The output of the ALM2402 goes as high as about 0.8 V and stays there in spite of the input. The DC-DC converter outputs nothing.
Analog is not my strong area, so I was wondering if you could provide a voltage follower type circuit that would give higher currents. Remember that one amp only supplies current while the other sinks it.
Thanks for any pointers, Dave