Part Number: USB2ANY
Hi,
The USB2ANY documentation specifically states the pitch of the output IDC interface is 50mil (1.25mm) on page 3 of SNAU228 (Jan 2018).
However, I have checked against many TI eval boards that contain a USB2ANY IDC header, and they all use a 2.54mm pitch IDC header.
Just as an example:
- TPS55287Q1EVM-085
- ULC1001-DRV290x
- TPS55289Q1EVM-011
I could not find any eval modules using a 50 mil (*1.27mm*) pitch header for the USB2ANY interface.
I have also seen that a 1.27mm pitch ribbon cable was recommended for use with the USB2ANY which adds to the confusion (refer here).
I am looking to include the interface header in a development board I am working on so clarity would be useful. I don't have a USB2ANY just yet for me to check myself.
Thanks,
Matt