Part Number: VFC32
Hello guys,
One of my customers uses VFC32 for their mass-production products.
Also they are going to use VFC32 for their next products too.
At this moment, they have the following questions to confirm if their understanding
about VFC32 is correct.
Could you please give me your answer top the follwoing questions?
Q1.
They use 20kohm for R1.
From Equation 1, VFS = 20kohm * 0.25mA = 5V.
They use 220pF for C1.
From Figure 2, Capacitor Value Selection,
fFS = (33000pF/(220pF + 30pF) = 132kHz
Are these equations correct?
Q2.
The measured value at 5V was 122kHz. There is a difference between the measured value and the calculated value. Is this difference mainly due to IC variation and RC variation? Or is the calculation formula incorrect?
Q3.
Does C2 affect the output frequency?
If there is no C2 value that matches the value shown in Figure 2, is it better to choose a larger value, or a smaller value?
Your reply would be much appreciated.
Best regards,
Kazuya.