Part Number: OPA2673
Other Parts Discussed in Thread: OPA2674
We are using the OPA2673IRGVT as a line driver for a Power Line Communication Application. We experienced several breakdowns in AC Line Applications of the chip with the following symptoms:
- OUTA / OUTB not functional
- Short Circuit on VS+
The Line Driver is supplied with 12.2VDC and has a 4.7Ohm Resistor in Series on OUTA / OUTB to the Power Line Transformer.

It appears as if DC line application do not cause the OPA2673IRGVT to fail, so first guess it is AC related.
Is the OPA2673IRGVT highly susceptile to input voltages of higher than 12V on the OUTA / OUTB (let's say disturbances from the AC main) and could this cause a short circuit on the VS+?
How about the absolute maximum supply voltage rating? It is said to be 13V, but recommended is again 13V? A 12V supply should be far enough from 13V or would you recommend even more safety to not damage the component?


The datasheet states, the the Pins (and I guess also OUTA / OUTB) are ESD protected. Is it likely that continous spikes from the AC Line could not be handled by the ESD Diodes? To me it looks like the ESD protection circuit are 2 simple diodes to supply and GND.

Is there a chance to send the defective chips to TI for research?