INA183: schematic check

Part Number: INA183

Hi Team,

since we change the solution from ADI MAX9634T to INA183A1, could you please help us confirm whether any change required to the current circuit or if have any recommendation?

we have review the circuit and , so far, we don't see any obvious issue.

OCP CIRCUIT - (1).pdf 

  • Tommy, 

    Everything looks in order, with the exception of their capacitor CB8L1 on the output of the device. They have chosen 22nF, where the maximum lissted in the datasheet is 1nF:

    If they need this much capacitance in the application for some reason, I would recommend they populate a small resistance on the order of 1-200Ω in series to isolate the output from the capacitor, or they can simply reduce the value to something <1nF.