Other Parts Discussed in Thread: XTR106
dear freinds ,
i have some problem with XTR106 current transmitter .my current output is 13mA to 28mA ,also this is not linear but i want linear 4 - 20 mA output ,there is no offset or span options in this ic like XTR 110. .please help me to get this output , one more thing is i am using function generator for giving input of 0-20mV to the ic instead of bridge.