This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LMH6554 is a 5V FDA with very good bandwidth and distortion performance.
The LMH6552 is a 10V FDA that is not quite as fast as the LMH6554 but it may be adequate.
Because of their excellent performance we have customers who use DVGA amplifiers in fixed gain applications we also have a dual PDA (programmable differential amplifier).
Parts that have performance similar to what you are looking for are the LMH6517 and the LMH6882.
Hello Eli,
I do not have a table of specifications of the LMH6882 compared to the AD4930. Looking at the AD4930 datasheet it looks like the LMH6554 is the best part for the desired performance. Why does the customer need a dual? Is it board space?
What sort of volumes are predicted for this opportunity?
Hi Loren,
The P.N is ADA4930-2 , two Amp's in one package : this is mandatory due to mismatched problems.
Forecast is 5KU. Additional TI devices for this project:
ADS5402I
LMK04828
DAC37J82 / DAC37J84
Power
B.regards
Eli
Hi Eli,
I rechecked our website and I can only find the following dual amplifiers that have good 500MHz bandwidth.
LMH6882
LMH6517
LMH6521
I think that if the LMH6882 does not meet linearity specifications it is hard for me to recommend anything else. The LMH6517 and LMH6521 would have a lot of noise at a gain of 1 or 2, although these amplifiers are very linear and have excellent bandwidth.
We have considered a dual LMH6554 in the past. I will forward this request to our marketing department for future product development.
Loren