This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
TLV274 common mode input range is Vdd - 1.35V as datasheet. TLV274 is RRO opamp. But we used it as RRIO opamp and did not experience any problem.
We used +-5V split suppy. I can measure excessive commom mode voltage on device pins. But everything seems working properly.
TLV2374 is pin compatible with TLV274 and it is RRIO but gets $0.30 extra cost. (totaly 5*$0.30) I can use TLV2374 but do I realy need to replace ?
Everything seems ok but I can not able to be sure. I can measure 4.87V and it is slightly higher than 5-1.35V.
Does anyone have an idea ?
Regards.