Other Parts Discussed in Thread: OPA549
Hi all,
Because my old power supply released the magic smoke, I decided to build another one, but this time in needed to be digital.
So after searching the internet I came across the OPA549 power amplifier and looked ad the datasheet and found a perfect example see picture 11.
With the OPA549 I also use a MCP4922 DAC to provide the voltage and current adjustment. But I have problem. The voltage can be controlled very good im kind of surprised to how well it controls the output voltage. But for the current limiting it does not work at all, and Im not sure where to look.
The voltage that is provided at the V+ (10,11) is about 33.6VDC, the V- (5,6,7) are connected to 0VDC. The output of the OPA549 is connected to two diodes as per figure 8 including the carbon 10 Ohm resistor.
The OPA549 has a gain of 10. the voltage and current setpoint is provided by a voltage that comes from the DAC MCP4922.
Now for example:
Vout is set to 13.8VDC (1.38VDC -> dac output)
ILIM Is set to 3A ore (3.33VDC -> dac output)
Output load = Car light 12V 55W.
The resulting current would about 4A (55 / 13.8 = 3.98)
what I measure with my ampere meter is that the current peaks ad 3.018A and then continues to drop to about 1.745A. which is not what I expected. What I do expect is for the current to stay at 3A and drop to another value.
But what is even stranger is when I set the current limit to 5A which is above the calculated current draw, it only allows 2A to flow. you can even here the OPA549 make some sort of sound (Some sort of buzzing) which would indicate that current limiting is active.
Another scenario is when the output voltage of the dac is set to 0.016V which is (0V) the you would expect a current draw of about 4A but it does not you can still here the current limiting active.
I don't know what going on here maube you can help me out with this problem.
If you need any schematics please let me know.
Regards Jordy