This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any data available?
The IVC102 data sheet only gives a typical graph which shows 0.6 pC for large input capacitors. No mention is made of the charge injection tempco.
Can I assume that the IVC102 charge injection tempco would be similar to that specified for the AFC2102?
The AFC2102 hold to integrate charge injection is 1 pC max (0.2 pC typical) with a typical tempco of 0.4 fC/C degree. With just the typical data, I calculate 0.4 fC/0.2 pC= 2000 ppm/C degree.
Can I expect the charge injection to cancel because I must both open and close the input switch each cycle?
Thank you