This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I need to operate the AMC1200 termporary with only VDD2 powered to 3.3V. Will that have any negative impact on the Vdd1 side? Vdd1 would be completely disconnected (floating ground and no Vdd).
Thank you,
Scott
Hello Scott,
Temporarily operating the AMC1200 with only VDD2 powered to 3.3 V will not have a negative impact on the VDD1 side provided that the absolute maximum rating of the AMC1200 are not exceeded.
Best regards,
Jose