Other Parts Discussed in Thread: MPY634, OP27
Hi, i have done a simple divider wiring as per datasheet. Now problem is that even if random fluctuations are there they should be at constant levels throughout the entire ranges of input. What is happening that the error is varying linearly with respective changes in numerator and denominator and we are unable to average it out. Regarding trimming suggestions , shall I give trim to Y1 input or Either of denominator X input? Shall i give trim via 470K and 1K resistance which is shown in other circuits other than divider? My wiring as per simple divider connection is all good and Y1 is connected to ground since I dont want anything to get added.