Hello E2E,
I am trying to build an amplifier using OPA549s in parallel configuration. I've attached a schematic. In prototype, I'm having an issue where the amplifier is oscillating when the set point is positive such that the amplifier is sinking >~7A and when I have more than 10,000pF switched in. This instability is not present when the amplifier is sourcing current and is present even if the load is purely resistive.
This design is an extension of an older design, using only OPA549 amplifiers, that design had a maximum capacity of 7A and was stable over the whole range of feedback capacitors.
Any thoughts of things to check or clarifications I can make?
Thanks
-Pete