This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i use RT- mode and diode mode to calibrate my real sensor twice .but the result is not right ,especially GAIN DAC and ZERO DAC is too large.for example GAIN DAC 3.83,ZERO DAC 2.20.who know reasions?
Hello Yao,
Could you please explain to me how you're calibrating the sensor? What connections are you using on the PGA309EVM and how are you generating the pressure and temperature signals?
Best regards,
Ian Williams
Linear Applications Engineer
Precision Analog - Op Amps
hello Williams.
thank you!
firstly i connect one real sensor to TEST board port:T1,T5,T4,using pga309 internal ADC sensor
connections : signal+_________T4:Vin1
signal-_________T4:Vin2
Vexc___________T1:Vsensor
GND___________T1:GND
JMP setting: JMP4:ext
JMP5:ext
JMP12:Vexc
JMP17:ext
and then put the board into fridge or oven.
i set three calibrate temperature point .10,25,45.and also have two weight load 250g 500g.
At first i put the board into fridge,hang nothing on sensor when temperature reach 10 degree,then hang 500g weight load,and next steps follow the powerpoint you supply.Moving the board into oven after finished temperature calibration at 10 degree, Not cut off the power supply when moving.
Voltage target setting is max 4.5V MIN 0.5V
there is part of my calibrations:
Vout max Vout min GAIN DAC
29 4.2875 0.05544 3.910
40 4.1980 0.05544 3.8749
45 4.1973 0.05559 3.8820
i am confused.I think GAIN DAC is wrong,because it over scale
could you give me a right connections that use real sensor with internal TEMP sensor mode on test board .
my sensor have four line: Vexc GND, Signal+,Signal-.
Best regards
Hello Williams,
I use PGA309 EVM to calibrate my real sensor.the picture is below
i prepare one fridge and one oven,also prepare weight for 200g,500g,50g;
using internal Temp sensor of PGA309;
the calibration steps is:
1.set three degree 10,25,45 ;and then put the board into fridge,hang nothing on sensor when temperature reach 10 degree.then click continue. next hang 500g on sensor after finish last step. the following steps according the powerpoint you supply. JMP setting that you have teached. I am not cut off the power supply when moving the board from fridge and putting the board into oven.
the calibration result is not right,for example Voltage output in my Pre-Cal Max voltage is 4.5
min voltage is 0.5
but my calibrations is : max 4.36 min 0.0554
especilly the value of GAIN DAC ,my GAIN DAC value over the scale of right.right GAIN DAC maybe 0.6.but my GAIN DAC is 3.8,