Other Parts Discussed in Thread: XTR110
Hello there.
I need some help in troubleshooting a problem we are having with the XTR110 V to I Transmitter.
We are experiencing repeated failures in Production of an XTR110 current source.
This design has been in production for several years now and the problem is not new.
The failure occurs at a constant rate, maybe 1%, but it causes us to scrap an entire board after much testing/calibration, so it is a costly problem.
The XTR110 circuit is configured for 0-5Vin and 0-20mA out as shown within Fig-1 of the datasheet.
The failure exhibits two features:
1) a loss of FET drive control (pin14 pegs at a low voltage, ~2V);
2) what appears to be a high internal current (part gets hot).
Whatever has ocurred, it appears to be a catastrophic failure.
The input circuitry appears to be unscathed and behaves appropriately - monitoring the output of pin8 gives expected voltages over the full Vin range.
The circuit was designed to operate at 12V, although the Vcc min specs at 13.5V.
Burr Brown was consulted at the time of the original design (10 years ago), and the green light was given for 12V operation.
Also, the circuit operates at a constant 73C temp.
Since the TI acquisition, has the XTR110 undergone any die revisions?
At the given operating parameters, 12V & 73C, are there any conditions that would cause the failure described?
Thanks,
Mark Abraira