This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Am using 14 pin version of LM2907 IC. Input frequency is RPM feedback from a tachometer. Maximum input freq expected is 13 kHz.
Circuit works fine over full range of frequency with square wave input with 50% duty cycle.
Practically, tachometer feedback thru optical pulse pick up then converted to electrical signal fed as input signal to LM2907 which has >80% duty cycle.
Ref Voltage at 11 Pin :1.2 V
Input freq signal amplitude 0 - 3.3V.
Supply Voltage :24V
C1 :470pF, R1: 10kOhms.
With 80% or more duty cycle, output voltage saturates around 3kHz frq.
Please help me out to solve this.
Thanks & Regards,
Chandan N