Hello everyone.
I have not been able to find any TI documents to help with this question. If there are some available, please advise, thanks.
I am requesting XTR110 industry standard suggestions for a 0-10V 4-20mA interface from an Eaton VFD analog output to an Allen Bradley PLC input using this chip. I had previously implemented it using discreet components but was dissatisfied with the linearity and thermal stability. Although the XTR110 replaces almost all of the circuitry I had designed, I am concerned with industry standard implementation and protection of the device in student workstations.
I am including the basic circuit with the following questions:
Recommended parts for through hole implementation:
Clamp diode to protect A1 from -.5V at pin 4
A suitable external mosfet that is not in a to-92 package (I can not find this from available recommended parts)
A suggestion for protection of the external mosfet drain which is wired directly to the PLC analog input card
Please take a look at my simple implementation and make suggestions.
Thank you very much.