Other Parts Discussed in Thread: XTR111
Hi all,
i use the XTR111 for getting a 4 to 20 mA output current in a product, which i am developing. When i measure at Vin and the output current over temperature i get sometimes an unclear behaviour of xtr111 and a very high output current drift.
Sometimes means, that not all XTR111 have the same issues.
For example
When i measure at 85°c it is possible, that Vin become higher and the Output current decrease.
When i measure the output current of an other test PCB with XTR111 on it, which was created by a colleague, the output current drift can be 100µA by increase the enviroment temperature to 85°C.
I was not able to recognize the problem with the help of the datasheet and the calculations in that forum.
Have anybody some hints for me.
Kind regards
Torsten Rehwald