This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm looking for a 4-20mA driver IC or reference design for a 4-20mA driver. Communication to the IC using SPI or I2C. Ideally the IC would support via a software command different outputs : 4-20mA, 0-20mA, 0-10V and 0-5V.
Also, the IC should have feedback or self compensation to maintain its current or voltage if the load changes.
The power source is a single supply +24VDC.
The application is driving a VFD control signal from our industrial control box.
We ultimately need 4 outputs, so the IC can have 1, 2 or 4 outputs.