This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Datasheet of TL07 family mentions the output swing typical value to be +/- 13.5v but nothing has been specified for Maximum value of output swing, can anyone confirm that? Page 6 of datasheet
regards
Thanks Ron for the reply, could you please also confirm if i am correct to say that the differential voltage (mentioned in absolute maximum ratings section)
Absolute ((VIN+) - (VIN-)) should be maximum 30v ? regards Siddharth
HI
i tried to search in the datasheet of TL07 series but couldn't find Isc -
What is the output short circuit (Isc) current of TL07 series opamp?
regards
Siddharth,
Short circuit current come from the supply rail then there is a 1.5V head room (drop out) reduction, lastly there is a 200 ohm resistance to the output pin.
When output is trying to go high, Isc = (Vcc+ - 1.5V - Vout) / 200 ohms
When output is trying to go low, Isc = (Vcc- + 1.5V + Vout) / 200 ohms
Siddharth,
The 200 ohms output can be calculated by choosing two points on figure 6 and doing math.
It is also seen in figure 13, 64 + 128 = 192
Thanks for the reply, so can i safely assume that internal resistance between VCC+ to output is 200 ohm when output goes high and similarly from VCC- to output is 200 ohm when output tried to go low? regards
Siddharth,
Meet me halfway. What is your maximum VCC+ and VCC-? To what is the output shorted? (ground or some other node?)
thanks
VCC+ is 12v and VCC- is -12v
you can let me know for the worst case - like when the ouput load tends to 0 or output getting shorted to ground
please can anyone share the output voltage versus load current curve for TL07 series of OPAMP
Thanks Ron for all the help, i would also request you to please provide the curve for +/-15v case and single supply voltage case from 0-30v. It will be great help thanks
Hi Ron, request your feedback over the data for +/-15v and 0-30v, hopefully the Lab results hae arrived