Part Number: LMH6629
Other Parts Discussed in Thread: TINA-TI, OPA857, TIDA-00725, TIDA-00978
Hi,
My customer is evaluating the LM6629 as Trans-Impedance Amp.
However, they could not get enough gain@120MHz on their board.
Though they're aimming 2000V/V, actual gain value is 680V/V.
They suspect that the cause is the pattern layout, because it can seem to get the gain 2000V/Von TINA-TI.
Could you support their following request if you have evaluated the LM6629 as TIA?
1. How is the GND pattern of TIA routing?
2. Should we countermeasure anything to reduce the input capacitance of TIA?
3. Could you tell the APD's name if you have evaluated the LM6629 with the APD?
And how do you measure frequency characteristic of APD?
APD: Avalanche Photo Diode
Additionally, I'm requesting their schematic and layout to my customer.
Please let me know if you need more information.
Best Regards,
Kuramochi