Part Number: TL3016
For some reason, E2E will only let me put this in the High Reliability Forum. Don't why, seems like a bug, please move as needed.
Our customer is powering the device from +/-5V. In this particular circuit, during a transient event the inverting terminal could get clamped to one schottky diode drop beyond the power supplies.
Will this cause phase reversal or any other non-ideal behavior?
The non-inverting terminal will within -2V < V+ < +2V.
Also, there is still confusion about the LATCH ENABLE logic. I see in the old internal forum that the data sheet was going to be updated with this language on the cover sheet,
"The TL3016 is an ultrafast comparator designed to interface directly to TTL logic while operating from either a singe 5-V power supply or dual +/- 5-V supplies. It featuress extermemly tight offset voltage and high gain for precision applications. It has complementary outputs that are latched when the LATCH ENABLE input is held high. For flow through applications, the LATCH ENABLE pin must be held low."
But apparently the data sheet was never revised.