This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to get all the gain Av configurations, using table 1 and table 2, also using equation 3, 4, 5, and 6 from the datasheet; however, I could not come up with the unity gain (Av =1) or half gain (Av=0.5). All the math and calculations did not give me Av=1 or Av=0.5
Does this part LMH5401 even support unity gain? or half gain?
Any help please?
Thank you.
Sincerely,
Nhan Nguyen
Hello Nhan,
The LMH5401 does support unity gain however, it requires some extra care. There is a reference design that illustrates this.
For gain less than 1 you need to be aware that the amplifier feedback resistors create a bypass path around the amplifier, so gain below 0.5 is not practical.
www.ti.com/.../TIDA-00522
Regards,
Loren
Loren,
Thank you so much for your feedback. I am also looking at this post https://e2e.ti.com/support/amplifiers/high_speed_amplifiers/f/10/t/391312 but I don't see any configuration for single ended input, and that is what I am interested in. So I am investigating more on the single ended input and single output. I may have more questions later.
Again, thank you for your help.
Sincerely,
Nhan Nguyen
Hello Nhan,
The LMH5401 datasheet has several examples of single ended configurations. Figure 56, 59 and 60 all show the LMH5401 with single ended inputs.
I would also suggest you use our free simulation tool TINA-TI to simulate your circuits so you can see how they work.
www.ti.com/.../toolssoftware
Regards,
Loren
Hello Nhan,
While it is technically possible to use the LMH5401 as a single ended output amplifier there are several drawbacks. We did not characterize the device with single ended output, so there are no performance curves that you can use to predict performance. See my blog post for more details:
Differential to single ended: What happens when you use only one differential amplifier output
Regards,
Loren
Hello Nhan,
The blog post seems to have suffered some formatting problem. I am attaching the article in PDF format so that you can see the inline equations.
{EDIT - Changed attachment to PDF for more universal access}
Regards,
Loren
Hi Loren,
For the LMH5401, if I was using +/- 2.5V supply with SE input, could I set the VCM to 1V (instead of 0V) to offset the outputs? It's kind of shifting the output without actually using a level shifter. I have the circuit in TINA and was simulating it. It took a long time, but after a while, it actually completed and the result is exactly what I was expecting (the outputs are 1V offset). I just wonder if setting VCM to a different value other than 0V (given +/- 2.5V supply) is OK or not.
Another question is that I have the output of the LMH5401 going into a LT part, which is a comparator LTC6754. How would you go about simulating these two chips using the same SPICE simulator (either LTSpice or TINA)? If using TINA, is there a way to import the LTC6754 spice model into TINA? or vice versa?
Thank you very much.
Sincerely,
Nhan Nguyen
Hello Nhan,
There are charts in the LMH5401 datasheet that show performance as the Vocm voltage is shifted from mid supply. Since you are driving a comparator it is likely that you don't care about distortion, if so the TINA simulations are going to be fine.
I'm not expert on importing SPICE models into simulation tools. There should be online instructions for importing SPICE models into both TINA-TI or LTSPICE. You should pick the tool that is most suitable for your purposes and follow the instructions for importing the necessary models. I have included a link that shows how to import a model into TINA-TI
Regards,
Loren