Part Number: LM139
Other Parts Discussed in Thread: TLV1704, TLV3404
Currently have the below circuit, which should take a 5V input on the non-inverting input, 2.5V on the inverting. However in reality, the non-inverting can only ever reach 3.7V and when used over the temp range the Opto isolator is sinking more current so the input voltage on the pin can eventually reach a state where the output of the LM139 switches states.
Doesn't create this scenario on the other devices in the quad package. If we remove the device then the voltages can be measured as predicted. Its only when this device is in circuit
any idea why the input on pin 9 would act like this?