Part Number: XTR111-2EVM
Other Parts Discussed in Thread: XTR111
Even though the eval board says it can take an 8-40V power supply the pdf says to set it up with a 24V ps(?)...
Question1: If I use a ps other than 24V do I need to adjust R6 to still get 4mA out w/0V Vin? (and what is the formula to do so?)
Question2: I see how to set Rset so that my max Vin = 20mA Iout but how do I setup the eval board such that my min Vin = 4mA Iout?
(ie I may have noise...) Would I change R8 to squelch my noise and then readjust Rset?
I have read the eval board tech pdf but admittedly only to pg12 of the XTR111 tech pdf which explains things in greater detail...
Thank you!
Best,
P