This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm an amateur Electronics Buff and still learning the basics. I'm presently trying to design my own Audio ADC Device. Based on the TI INA2137 Audio Differential Line Receiver. I want to make a Mic Pre-Amp and USB interface for Computers. I plan on using the MSP430 Prototyping Boards, that I already have. I have 3 and two of them have the Anaren Wireless Modules on them. I would like to build two different, setups. One Wireless. And one Wired, Sending Audio into the Computer, via USB. To send the Audio into a Computer, for Recording. If this will work. I also bought, LM1085IT-ADJ/NOPB-3A Fixed Adjustable Output Linear Regulator and LM3525M-L/NOPB-Single Port USB Power Switch and Over-current Protection. In case I need to build the whole Circuit from scratch. I don't know if I need to add Resistors to the Circuit or not. Since the INA2137 has some built in. I've spent over a week. Researching Circuit Designs, for this Chip. But, have only found two, general Designs. On other Web Sites. Do you have any experience, Designing Circuits with these Chips, that you could share with me?
Thanks,
Don