Part Number: OPA2141
Other Parts Discussed in Thread: OPA320, OPA350, OPA340
Hello.
I am using OPA2141 as a follower to increase the input impedance of the microcontroller´s ADC. All is ok if the (+) input is tied to GND or is tied to a voltage, but if the input is left floating, I see 0.9V in the OP Amp output. Is this a normal behaviour? I have attached an image where the circuit I am using is described.