Part Number: OPA369
Other Parts Discussed in Thread: OPA320, OPA191, OPA316
I'm using an Invensense ICS-40619 MEMS Microphone which has a differential output and (in low power mode) a differential output impedance of 5.5 k Ohms and an output level approaching 0 dBV at 130 dB SPL input). The Invensense datasheet insists that the differential outputs need to be isolated with 2.2 uF (minimum) caps. My application will sample the ADC input to gather data that will be used to capture low frequency signals (50 - 100 Hz) and I'm thinking that gain in the range of 5 to 10 times will be needed.
I'm looking at the OPA369 datasheet and wondering if I can use it in the way shown in the circuit below, not sure if I need C1 and C2 is clearly providing frequency rolloff. One issue is that I want all of this to run off a single rail supply of +1.8 volts.