This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.Why the amplifier will be consuming more current than normal and self-heating when it rail out?as is saying in《Properly terminating an unused op amp》Fig.2(a)
"The circuit in Fig. 2a connects both inputs together and to GND, but it ignores the effects of input offset voltage (VIO) between the inputs. Depending on the polarity of VIO, the small voltage between the inputs causes the output to drive to one supply rail or the other. Since this circuit has large open loop gain, the output saturates and the device consumes extra current. This implementation should be avoided."
if the ampilfier is of JFET-input, its input current is as low as nA, and output current is 0A, why the OP can consume much current, and where is the current loop?
I'm sorry, the OP number TL082 maybe confuse you, it only just a example.
what I want to know is the description of ”Properly terminating an unused op amp”,why OP will consume extra power when it rail out?
"The circuit in Fig. 2a connects both inputs together and to GND, but it ignores the effects of input offset voltage (VIO) between the inputs. Depending on the polarity of VIO, the small voltage between the inputs causes the output to drive to one supply rail or the other. Since this circuit has large open loop gain, the output saturates and the device consumes extra current. This implementation should be avoided."
in the following site:
can you open it?
in anohter book, “OP Amps for Everyone(3rd edition)”, similar discription is also found.