Part Number: THS4513
Other Parts Discussed in Thread: THS3095, , TINA-TI
Hi,
I'm trying to simulate a circuit using a THS3095 followinf by a THS4513 and I have some questions.
First stage is a unity gain non inverter THS3095 to buffer my signal. After this stage, signal is good but the common mode of my signal is not the common mode of the second stage, based on THS4513.
The aim of the second stage is to convert the single ended signla into differential one in order to drive an ADC.
I prefer to avoid of setting the common mode on the output of the first stage because high and low levels of my signal can vary so, I tried to AC coupled the two stages but it's not working.
It works correctly if I DC coupled the two stage and set the common mode of the signal at the output of the THS3095 at the same value than the common mode of the THS4513.
I just want the same signal as the output of THS3095 but in differential mode 0V centered.
Could anybody explain me what is wrong, please? Regarding the Datasheet, it seems to be working.
Thanks
Matthieu Baque