Part Number: LF398-N
I have been using the TI LF398-N in one of our products for many years with no problems, however our most recent production batch do not work correctly due to excessive input offset in all three LF398-Ns used in the circuit, normally there is less than 3mV difference between input and output, now there is about 15mV. The standard offset adjustment circuit described in the datasheet no longer fully zeros the offset, I changed resistor values to achieve zero offset, but then the offset varies with signal voltage. Swapping the ICs with some old ones from stock solves the problem, but I have no more in stock. I tried changing the LF398-Ns for the -AN version, but these seem to have the same problem, Is this a known issue? Is it just a bad batch of ICs that I got from RS components? I would appreciate any help or advice.