Other Parts Discussed in Thread: AMC1301, ISO124
I want to use AMC1301-Q1 to isolate analog signal.The input range of AMC1301-Q1 is ±250mV,and fixed-gain is 8.2. But table 6.1 indicate the range of VINP is (GND1-6) to (VDD1+0.5). Please help me if I can use it to isolate analog signal with the frequency if 10kHz,amplitude is 5V,and not difference???