Other Parts Discussed in Thread: AMC1200, THS4551, THS4131, LMP8350
Hi,
In my application I need to sense the load current from isolated 300VDC. In order to do that, I used the TI "AMC1200" with floating supply (to the 300V) and with 5V supply (to logic- analog). Now I need to drive this signal with over the ~70cm between cards, twisted pair and shielded. In the other curt I will have a precision, fix 0.4 Gain, Fully Differential Funnel Amplifier that drive switched capacitor inform of a Σ-Δ ADCs with precision to ~18bits. To make my application more robust I need a fully differential input stage amplifier with gain 2.5 (that will connect to the AMC1200 output) that can drive the twisted 70cm long and the Funnel Amplifier (with ~18bits or the closes to that). Can you recommend such an fully differential precision amplifier? Operation Temperature must be at least 105 degree.
In addition, is it possible to use the AMC1200 as a driver for the ~70cm between cards or should I use different driver (ignore the 0.4V gain on the other card, let's say I can use it in unity gain)? What it the parameter that effect the driving thought the ~70cm twisted pair, shielded lines)?
The project ADC volume is ~2000 chains.
http://www.ti.com/product/AMC1200/technicaldocuments
Thanks,
Idan