Part Number: THS4551
Other Parts Discussed in Thread: ADS127L01, TINA-TI
Hello,
I have a rather unique problem. I am going to use a THS4551 as a differential adc driver for a ADS127L01. My issue is the stage before the THS4551 is a trans-impedance amplifier that will have a 0V to 10V output. The output will also be offset by a known DC voltage. So in this scenario, I will use the voltage offset as the sudo differential negative input and the TIA output as the positive input and both need to be attenuated by 1/4 so the TIA output can map to the ADC range.
You have a reference design for driving the ADS127L01 in your datasheet,see below. I would like to know how to modify it to get the 1/4 attenuation on both the negative and positive inputs but not change the frequency response. I assume a simple voltage divider will work but I am new to FDA and Im not sure how to calculate the input impedance to get the attenuation right. Plus an resistance I add to the source will change the filtering properties.
Thanks,
John