This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using INA326 to amplify signals from a load cell, Vdd=3.3V, I want to set output voltage wrt vdd/2,(considering load cell movement in both directions). In the datasheet suggested circuit is fig 2. But with this circuit, i am getting output voltage as 954mV.and according to figure 1, the output is exactly at vdd/2(which is correct), At balanced conditions.
So, which is the correct circuit, fig 1 or fig 2?
Vishal,
The circuit in Fig 2 is the correct one for G=2,000 and it works as intended - see below. Check your connections or modify the schematic I attached in this post.
Vishal,
For most traditional three op amps voltage feedback instrumentation amplifiers, they MUST have Vref driven by low impedance source or be grounded but INA326 is different. Because of its current feedback topology, you either have to drive pin 5 with voltage divider for output referenced to Vcc/2 as discussed previously or connect R2 to ground - see below both cases.