Part Number: LM318-N
Other Parts Discussed in Thread: LM318
Hi,
The schematic below is circuit for a measurement control application, one of my main customers.
It seems blurry because resolution is not good, but please ask for a review.
thanks,
TS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ron,
thnaks for your help.
Below is more detail infomations.
U12, U11 component margin review
- Proceed with component margin review through waveform measurement in normal circuit.
1) Waveform measurement and margin check for U12 part
(RMS, MAX, P-P, MIN is measured value.)
| PIN | REF | DATASHEET(MAXIMUM) | RMS | MAX | P-P | MIN | MARGIN VOLTAGE(calculation) | Remark | |
| 2 | IN- | ±15V or midium value of VCC | 1.22 | 3.2 | 5.3~-24.7 | in spec | |||
| 3 | IN+ | ±15V or midium value of VCC | 0.833 | 3.7 | 5.3~-24.7 | in spec | |||
| 4 | VCC- | -20V | -24.4V | -29.7 | in spec | ||||
| 6 | OUT | -21.57 | 5.2 | 27.9 | -22.7 | - | |||
| 7 | VCC+ | 20V | 5 | 12.3 | in spec |
* Input range calculation
1) midium value of VCC : -9.7V((-24.4+5)/2)
2) Maximum range of VCC
- VCC+ : -9.7 + 20 = 12.3V
- VCC- : -9.7 - 20 = -29.7V
3) Maximum range of VIN
- VIN+ : -9.7 + 15 = 5.3V
- VIN- : -9.7 - 15 = -24.7V
Oscilloscpe capture for each pin of U12
2) Waveform measurement and margin check for U11 part
(RMS, MAX, P-P, MIN is measured value.)
| PIN | REF | DATASHEET(MAXIMUM) | RMS | MAX | P-P | MIN | MARGIN VOLTAGE(calculation) | Remark | |
| 2 | IN- | ±15V or midium value of VCC | -20.15 | 5.3~-24.7 | in spec | ||||
| 3 | IN+ | ±15V or midium value of VCC | -20.18 | 5.3~-24.7 | in spec | ||||
| 4 | VCC- | -20V | -24.4V | -29.7 | in spec | ||||
| 6 | OUT | -20.15 | - | ||||||
| 7 | VCC+ | 20V | 5 | 12.3 | in spec |
* Input range calculation
1) midium value of VCC : -9.7V((-24.4+5)/2)
2) Maximum range of VCC
- VCC+ : -9.7 + 20 = 12.3V
- VCC- : -9.7 - 20 = -29.7V
3) Maximum range of VIN
- VIN+ : -9.7 + 15 = 5.3V
- VIN- : -9.7 - 15 = -24.7V
Oscilloscpe capture for each pin of U12
thanks,
TS
HI Ronald,
Perhaps this is my last question regarding this issue,
As you mentioned in the previous answer, you said that "The best capacitance is no capacitance. This is true of almost all op amps."
Can you explain this in more detail?
If you have any material or documents related to this, please share it.
Any advice is welcome.
thanks,
TS
TS,
I suggest the stability section of the precision labs vides for op amps.