This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, i am use lf356m now, the sch is above, but the gain is smaller when the input signal frequecy is low, the gain response is like above, the x axis is frequency, the y axis is gain, please help find out the reason, i hope that gain is same no matter the input frequency. thank you!
Part Number: LF356
Hi, i am using lf356m to design an amplifier, but i find that when the frequency is low, such as 10, 20 or 50Hz,the gain is much smaller than i hoped, the sch and gain response is like below, the x axial is frequency , the y axial is gain number. please help to find out the response, thank you.i hope that the gain is same no matter the frequency low or high.
Hi Ronald,
Thanks a lot for your help, i have changed the circuit as below, and gain works good now,
I don't want to amplify the DC component of the input signal, i want the low frequency cutoff is 5Hz, the high frequency cutoff is 2000Hz,
what i need to do to realize the above two cutoff?
the maximu output amplitude is less 1V.
Thanks again.
Michael Ding.
What was the lower cutoff with your circuit? It looks like 1.6Hz to me.
Here is a 7Hz to 2kHz modified version. Using free TI-tina