Part Number: OPA4277
Other Parts Discussed in Thread: OPA4227
hello.
I'm using the operational opa2477. I am using it within a circuit to adjust the gain of a signal. The amplifier gets very hot, so I remove all the components that connect it with the other parts of the circuit. In conclusion the amplifier is only connected to the + -12V supply, and its respective decoupling capacitors, but the amplifier still reaches temperatures of 60 ° C and above. Is this temperature normal for the amplifier? I have changed the amplifier twice, and the result remains the same.
the funny thing is that the amplifier works, and fulfills its task, but I do not know if I let the circuit work with this temperature, in a short time, the circuit no longer works.