Part Number: LM6171
Hi,
I have use the LM6171B for integrating a sinusoidal signal such that I can vary the amplitude and frequency of the input signal. The circuit which I have attached here is from TINA and for example, I have use an input signal with 1Vpp and f=5KHz. Therefore the output of the 1st integrator should be a cosine with an amplitude ~6.24Vpp and the output of the second integrator should be a sine with a phase difference of 180 degree w.r.t the input signal having an amplitude of ~3.9Vpp. However, since the gain setting is very large (R2 and R4), I'm not getting the results. Can you please suggest how to solve this problem?