This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hello,
I'm in the process of trying to model a unity gain follower using the OPA197 with various load capacitances but am running into some issues with TINA. Note that I'm a hobbyist, not an EE, so I apologize in advance for any dumb questions!
First of all - in the attached file "opa197 unity gain", which is just the simple unity gain follower circuit, I am getting the error "Convergence problem. Check the analysis parameters". I'm not sure exactly why its having difficulty with the circuit as it seems pretty basic...
Secondly, in the attached file "opa197 unity gain stability analysis", I've attempted to follow the instructions in this tutorial in order to get look at the phase margin for the circuit (). However, The curves that are being generated look very strange, and the baseline open loop gain seems to start from -50db... I'm not certain as to why the curves are coming out wrong (see attached image). Can anyone give me a hand?
Thanks so much in advance..
Victor,
Please see the attached circuit opa197 unity gain stability analysis_revd.TSC.
It is the same as your circuit except the power supply has been changed from a single +12V supply to two supplies with voltages of to +6V and -6V.
The resulting open-loop gain & phase - shown in the right-most top plots - are much closer to those shown in the schematic's original graphics.
The reason this helped is because the pins of the original circuit are at about 0V, which forces the simulator to bias the circuit for an operating point at ground which won't allow a meaningful signal swing.
By changing the power supplies to -6V and +6V, the 0V bias point is at the mid-point of the power supplies.
This is an optimum bias point from the standpoint and it allows the greatest amount of signal swing.
The other circuit seems to have an issue with the 500pF load capacitance.
If the load capacitance is reduced to 1pF, the AC response changes to the expected behavior.
The device data sheet makes some recommendations in Table 3 for values of Riso for given values of Cload.
Based on the table, I'm guessing the resistor between the amplifier and the load resistor needs to be larger.
If none of this helps, I can move this thread to the E2E Amplifiers forum that is monitored by the product experts.
Please let me know if that is what you want me to do.
Regards,
John
Victor,
At this point it would be best to weigh in with the product experts that monitor the E2E Precision Amplifier Forum.
I will move the thread to that forum and they can help with questions on the actual device.
Regards,
John
Hello Victor,
Thank you for your patience during the holidays. The OPA197 can operate just fine on a single +12V supply, however it's advised in this case to bias the input signals up to mid-supply (+6V) to make sure the amplifier operates in the linear region. If not you can see large offsets and incorrect transfer functions appearing when you try to verify the circuit behavior in simulation.
I've modified both of your original circuits to work better at single-supply by biasing the input signal to +6V. You can easily do this with a resistor divider if you have access to the +12V node on your board. The stability test with Riso = 10 and CL = 500pF had over 60 degrees of phase margin, so there should be no stability issues in that configuration.
opa197 unity gain stability analysis_ss.TSC
Best regards,
Ian Williams
Applications Engineer/SPICE Model Developer
Precision Amplifiers
Hey Ian,
So I implemented the precision reference buffer circuit on page 30 of the OPA197 datasheet. The banding is not entirely gone, but it has changed - and interestingly a couple of times, I've had some minor visual abberations appear after the set has been on for about 20 mins. I've noticed some shift over time in the banding before inserting the OPA197 buffer circuit which I presumed was temperature dependent drift in the gamma chip. This is different though - instead of worsening of a specific band on the screen, I'm getting some irregularity/streaking in the area of a band that appears after the set has warmed up.
Basically, what I believe is causing the banding (which is vertical stripes of slighly different color across the screen, several inches wide) currently is differences in the reference voltages seen by the vertical panel driver ICs caused by voltage fluctuations in the gamma voltages from oscillation from the gamma IC (which is designed by a company called Silicon Works in Korea, which doesn't supply a datasheet..). With this slightly different symptom I'm now seeing, I'm uncertain whether the buffer circuit is unstable with the 10uF loading suggested by the reference buffer design in context of the OPA197 driving a relatively long trace + ribbon cable, or if the filtering now in the circuit is only partial filtering the oscillation from the gamma IC on the board. I'm currently using a 75ohm isolation resistor to isolate the gamma chip from the ~foot of 24awg cat5 network cable I'm using to carry the input signals to the buffer board with the OPA197. Perhaps I need to increase that isolation resistor value in order to further quiet that chip..
Anyways - given I'm using 2x 4197s and 1x197 for the 9 channels, is there any reason they would be overheating supplying DC voltages to the buffer circuit, which may result in instability? Is the context of driving the trace/ribbon cable not ideal for this application?
Any thoughts would be greatly appreciated - unfortunately FYI I don't have a scope.
Thanks,
Vic