This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a product use the INA199A1DCKR to check the current. after the PCBA done and the hardware QC pass (contain the current check), it work normal, but when it ship it to our client, there are 2pcs PCBA has the issue, it cause by the INA199A1, the IN- to GND forward voltage is 0.144 V,and the IN+ to GND forward voltage is 0.7 V. I think it may damaged when it transporting or assembling, may caused by ESD? The schematic is according to the ddatasheet.,the battery is 7.4V. Is it has some problem on my designed? I hope you can give me some feedback, thank!
Hello Jiayu,
Someone from my team has pointed out to me that the A version of the INA199 does not have the most robust ESD protection. It is possible your client may have applied transients that exceed A version's ESD cell specifications. Fortunately our B and C versions of the INA199 have more robust ESD cells. More information on this particular issue can be found on https://e2e.ti.com/support/amplifiers/current-shunt-monitors/w/faq/3187.what-is-the-difference-between-the-ina199a-ina199b-and-ina199c-devices and https://e2e.ti.com/support/amplifiers/current-shunt-monitors/f/931/p/410196/1456777
Hello Patrick
Thank your feedback. Series with the shunt resistor contain a MOS and a small value resistor,it is less than 1KHz frequency to control the MOS, according to the resistor specification, the circuit instantaneous current may up to 28A, and the average is about 12A.
Hello Patrick,
The latest test result, if the INA199A1 damaged, it does not cause the circuit short,but it cause the leakage current, before the battery drain to 0V, it seem work normal, we will do more test about the damaged unit. but when the battery drain 0V, we can not charge it. so the may not our client operation error,it may damage when we solder battery or after. We now are looking forward some way to found which unit's current sensor is damaged, because we already Mass production. I hope your team can give some suggestion or feedback. Thank you very much !
Hello Jiayu, Zach,
The ESD protection of the B and C version is supposed to better and thus I would expect it to perform better. However, you still may need additional external protection in the form of a TVS or a large lossy capacitor between the battery and the INA199. If you decide to use a TVS, its placement or layout needs to be carefully addressed. The following article, provides some information on good TVS layout practices: http://www.ti.com/lit/an/slva680/slva680.pdf.
Patrick,
Thank you so much for your assistance. We will look into both of these options and hope they solve the issue. Thank you!