This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I rig up simple voltage feedback circuit using LM7171 OP AMP. Schematic looks as below.
UUT = 30V. with gain of 2. PIN #3 was floating. it is found after sometime (15 to 20 seconds), IC is getting hot. I didn't debug the circuit yet.
Kindy suggests what would be wrong in the schematic?
Regards
Kumar
Hi Jacob,
UUT =12V, I have connected the Pin#3 to ground for initial conditions. IC is not getting heated. I feel,12 volts is not issue. still testing with different voltage conditions.
UUT = 32V, even input Is connected ground, still IC is getting HOT. Not sure what will be the reason.
Output is not connected to any load. still IC is getting HOT. what could be the reason?
voltage range on the Pin #3 is 1.5 to 5V. with gain of 3 V.
Regards
Kumar