Part Number: TLC271
Other Parts Discussed in Thread: OPA170
this IC's in this configuration- can it be programmed or is met to be just a drop in part that should work as is
if it can be programmed how do I do it ?
it works like it is but I am getting a little DCmv on the out put of the power amplifier it is adjusting for
OH there is a -6.8v on pin 4 and + 6.8v on pin 7 and 115mv on pin 6,8 there is a 2.2 meg on pin 2 going to speaker outputs
thanks