This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I’m trying to make sense of the noise specifications in the datasheet for the LMH6559. In the table on page 3, the noise for +/-5V power supplies is reported as 5.7nv/rtHz@1MHz. But, in Figure 17 on page 11, it is much lower than that, more like 2.5 nV/rtHz@1MHz. What’s the right value to calculate with, the one in the table or the one in the figure?
Thanks and best,
Miri
Hi Miriam.
the original datasheet of LMH6559 from NS has a different value, 2.8nV/SQRT(Hz):
So, the 5.7nV/SQRT(Hz) could a typo.
Kai